This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63002

Other Parts Discussed in Thread: TPS63002, TPS63001

I believe that, there is some mistake at the design of TPS63002

The N-mosfet connected to L2 constantly goes to short circuit (PGND) after a few minutes/seconds of operation.

Input is 4.2V LiPO battery, and all of the design recomendations are in place.

However TPS63001 in parallel works just fine. (PCB designs for both are the same).  -> 2u2H for 3v3(001) and 4u7H(002) for inductances.

Any suggestion will be wellcomed.

Thanks in advance.

 

Very best regards,

Miro Tzonkov.