Other Parts Discussed in Thread: UCC25800
Tool/software:
Hi,
I need to power an Add-on card in a rack module with UCC25800. I choose this IC because of low inter winding capacitance so the EMI noise of one card will not affect the other cards in the system.
I have designed the circuit and it is working with satisfaction. The IC or the toroidal core is heating within 42°C, but the output diodes are peaking upto 53°C with natural air cooling. This may exceed 60°C+ with enclosure. Is it normal. What should I do to reduce the temperature.
My design parameters are as follows,
Input - 24V regulated
Output - 22V to 26V
Power - 4W (should capable upto 6W)
Frequency - 550KHz
Toroidal core - B64290L0044X49 (AL= 660nH, Primary inductance = 35uH, Primary turns = 7, secondary turns = 8)
I have taken most of the values from EVM schematic and wound the primary coil with inductance of 35uH which is near to the 26uH of reference design. Here I have attached the thermal image of the PCB. The core is in almost ambient temperature at 200mA output current. The IC is 42°C with very minimal thermal PCB track size and it can be improved in actual design. ES1D output diode is selected because of 15nS recovery and 7pF of junction capacitance. The diode has 200V and 1A rating where my output rating is only 24V@ 200mA.
What mistake I made here?. Is it the nature of the circuit or I should select a different diode with different parameters?
Udhay