Other Parts Discussed in Thread: BQ25895, , PMP40496
Tool/software:
Hello,
I’m developing a portable device based on the Raspberry Pi Compute Module 5 (CM5). The system is powered via battery and external supply, and requires up to 5A max output to power the RPi.
I’m evaluating the following Texas Instruments battery charger ICs:
-
BQ25895
-
BQ25883
-
BQ25731RSN
My key requirement is:
-
Support for 5A output (especially in OTG/boost mode or through the system rail)
Could you please help clarify:
-
Which of the above ICs can reliably deliver 5A output?
-
Does the BQ25895 or BQ25883 support this under any reference design (e.g., PMP40496)?
-
Is the BQ25731RSN more appropriate for this high-output requirement?
Any recommendations or application notes for achieving this safely are greatly appreciated.
Thank you!