Other Parts Discussed in Thread: AM6442, TPS650861, TPS650864, TPS65224-Q1, , TPS65219
Tool/software:
Hi team,
We are using AM6442 processor in our design. For the power supply section we had checked the eval board in which TPS6522053RHBR - PMIC IC is being used.
But for this IC the output current is very less. Please find the below mentioned current requirements and suggest a PMIC for our system.
The requirement is of integrated Buck converters and LDO's.
Buck Converters:
Vin = 2V to 5V ( 3.3 Nominal )
Iout = 3A
Vout = 1V to 2.5V
LDO's:
Vin = 2V to 5V ( 3.3 Nominal )
Iout = 2A
Vout = 0.75V to 2.5V
Kindly consider the above requirements and suggest a PMIC with 3 Buck and 4 LDO's or higher.
With best regards,
Teja.