Other Parts Discussed in Thread: UCC28951
Tool/software:
I'm trying to understand how to do frequency dithering according to the Application Report SLUA646. There seems to be an inconsistency with the orientation of the RT resistor (called R6 in the report). The Datashseet for UCC28950/UCC28951 calls for this resistor to be connected between VREF and the RT pin. In the report's Figure 1, this resistor is connected from the RT pin to Ground. In the report Figures 3 and Appendix 1, the resistor RT (R6) is connected from the RT pin to VREF. The report even says "With the controller set as a master, this resistor is tied from the Rt pin to the Vref pin which supplies a 5V source." Is Figure 1 wrong?