This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994QFNEVM: TPS65994BH:How can I edit the file f909.12.13 in USBCPD Application Customization Tool

Part Number: TPS65994QFNEVM
Other Parts Discussed in Thread: TPS65994BH

Tool/software:

HI 

 1.PD: TPS65994BH

    USBCPD Application Customization Tool:GUI build  version:6.4.32

2.We want to edit f909.12.13 ,it will report Input Base Image Load Disallowed(It is not permitted to load a base image file that is incompatible with the current open project.Current Open Project supports firmware version: f909.12.xx Selected Binary File firmware version : ffff.ff.ff),but edit  f909.12.15. is ok.

3.How can I edit the file f909.12.13,change GUI Version or use other methods,thanks