Hello,
We need a voltage inverter providing -7.0V 50mA. In the datasheet for the MC33063 there is an example showing almost this, but the input voltage is limited to +6.0V. Our input will be between +15 and +25V. Is this possible?
Following another thread, it seems like the important limitation is Vin-Vout, which in this case will be less than 32V (rating seems to be 40V), but are there any other restrictions?
Basically, can anyone please suggest the relevant changes to the schematic (Voltage-Inverting Converter, Figure 10.) in the datasheet so that it accepts a Vin 15-25V and provides a Vout of -7.0V at 50mA? Efficiency is not an issue, ripple is however (the suggested optional filter seems to do a good job though and that should be sufficient for me also).
Many thanks in advance!
Regards,
Staffan