This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73606: LM73606

Part Number: LM73606


Tool/software:

Hello

The Vin is 11V-17V and the Vout is 1V.

It is ok to connect the PGOOD to 3.3V and not to Vout. The Pgood should be power up other device with Vih>2.5V.

Roi