This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: Request for Schematic Review.

Part Number: TPS25947


Tool/software:

Hi TI team,

We are currently designing a circuit using the TPS25947, and would appreciate your help reviewing our schematic to ensure there are no obvious mistakes or issues.

Thanks!

  • Hi Tom,

    What is the input voltage for which this is designed. In the schematic, it is mentioned that the battery voltage is 6V to 8.4V. I am assuming this is 2s Li-ion cell. The UVLO, OVLO and PGTH are all set for 12V nominal application. Kindly ask them to change the resistive ladder values.

    Best Regards,
    Arush