Other Parts Discussed in Thread: BQ27542-G1
Tool/software:
What is the effect of setting BQ27542-G1 LFPRelax to 1 when applied to lithium-ion polymer?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
What is the effect of setting BQ27542-G1 LFPRelax to 1 when applied to lithium-ion polymer?
Hi Sir,
Excause me,
1. If LFPRelax to 1,What is the effect of setting BQ27542-G1 LFPRelax to 1 when applied to lithium-ion polymer?
2. We have completed golden learning before, what are the side effects if we change the LFPRelax bit from 1 to 0 and do not do golden learning?
Thanks
Hello Iris,
1. If LFPRelax to 1,What is the effect of setting BQ27542-G1 LFPRelax to 1 when applied to lithium-ion polymer?
-The feature when not be enable for lithium-ion polymer and the effect would be not being able to enable it
2. We have completed golden learning before, what are the side effects if we change the LFPRelax bit from 1 to 0 and do not do golden learning?
-If you are LFP chemistry cell and changing the LFPRelax bit from 1 to 0 the side effect is that the cell won't be able to maintain a full charge and Qmax could be incorrect.
For Li-ion batteries, should DODWT be set to 0 or 1?
For lithium cells this parameter is not needed but if you do decide to enable it, it would slightly improved the accuracy of the cell but this does mean that your relaxation period would have to be around 5 hours to be able to fully utilized it.
Thank you,
Alan