Other Parts Discussed in Thread: LM65625, LM65635EVM
Tool/software:
Hi Sir,
I would like to find a 60V/3A DC-buck device to customer, it must be has the small package and low thermal resistance, when the operating freq at 2MHz, Vin = 12V, Vout = 5V, load at 0.5A~1.5A, the efficiency up to 90%.
Could the LM65645-Q1 meet this request? if it cannot, could you advise a device to me? Thanks!