Other Parts Discussed in Thread: LM5143
Tool/software:
Hi expert,
Our project used the TI LM5143 chip, and during the debugging process, we encountered a problem. We have one power output set to 14V, and the schematic is attached. During the rise of the input power supply voltage, an abnormal output waveform is observed, exhibiting oscillations. When the input power is at 11V, the output is normal, and the waveforms of the upper and lower MOSFETs are shown in the figure below: yellow for the upper MOSFET and blue for the lower MOSFET.
When the power input is 15V, the output is abnormal. Under no load, the inductor heats up, and the output waveform is abnormal, as shown in the figure below.
Thanks a lot!