This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A47: About EN and NC pins

Part Number: TPS7A47

Tool/software:

Hello,

I am an FAE at a distributor that handles TI products.
I have received some questions from my customer about the TPS7A4701.
(Question 1)
It generates +5V from +12VIN.
If a voltage of -0.4V to 36V is applied to the EN pin while no voltage is supplied to the IN pin, is there a possibility that the device will deteriorate or be damaged?
(Question 2)
The datasheet states the following about NC pins:
"This pin can be left open or tied to any voltage between GND and IN."
What is the best way to connect them?
Is it better to connect all NC pins to GND rather than leaving them open?
Looking at the layout example in Figure 28 on page 21 of the datasheet, each pin is connected differently.

Best regards,

  • Hi,

    Question 1:

    It is beyond the recommended operating conditions but since it's below the abs. max rating you shouldn't expect deterioration or damage. Usually, I clarify that the datasheet values are only applicable to proper regulation within recommended operating conditions unless otherwise stated but if 0V is applied to the input, the undervoltage lockout circuit will disable the device regardless of EN state.

    Question 2:

    Typically, grounding the NC pins has a marginal improvement in thermal performance as it adds another possible thermal conduction path, so grounding them is slightly preferred. In this case it appears that we grounded the ones which makes for an easier, cleaner, and more thermally conductive layout when you feed the ground plane across them to connect the ground pad. 

    Best,

    Gregory Thompson