This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25946: TPS25946 Backup Battery Switching Application

Part Number: TPS25946
Other Parts Discussed in Thread: TPS25947

Tool/software:

Hi TI Team,

I’m currently using the TPS25946 to implement a backup battery switching function.
Please see my schematic below:

In the circuit:

  • The upper section uses BAT_IN as the main battery.

  • The lower section uses BACKUP_BAT as the backup battery.

My requirement is that when the main battery is present and supplying power to the load (BAT_VCC), the eFuse connected to the backup battery must be disabled to prevent it from supplying power.

To achieve this, I’m using the PG (Power Good) feature:

  • When the main battery is present, the PGTH voltage of the upper TPS25946 exceeds the threshold, causing PG to go high.

  • This PG high signal pulls the EN/UVLO pin of the lower TPS25946 low, thus disabling the backup battery output.

  • When the main battery is removed and PGTH falls below the threshold, PG goes low, allowing the EN/UVLO of the lower TPS25946 to go high, enabling the backup battery to supply power to the system.

Could you please confirm if this design approach is valid and recommended for this kind of application?

Thank you.

  • Hi Tom,

    I will check this and get back to you on this early next week.

    Best Regards,
    Arush

  • Hi Tom,

    This looks very standard way to implement the power muxing. Here, instead of using a FET to pull EN low, You can directly use the PG signal to OVLO pin which behaves like ENb.

    Also can you confirm which device are you using. Is it TPS25947 or TPS25946. Both are p2p but TPS25947 provides reverse current blocking even when on which is required in this application. TPS25946 won't work here.

    More details in TPS25947 datasheet section 9.5

    Best Regards,
    Arush