Part Number: TPS7B7701-Q1
Tool/software:
Hi TI Team,
We are using the schematic of the TPS7B7701QPWPRQ1 as shown below.

We have observed a phenomenon where, when the chip is in normal operation, briefly pulling EN low (e.g., for less than 1ms) causes the chip to enter latched-off mode, with the ERR pin pulled low and the output disabled, as illustrated in the figure below.

Upon zooming in on the waveform, we noticed that Vin briefly drops below Vout for only a very short duration (ns level), as shown in the following figure. Would the TPS7B7701 still enter latched-off mode under this condition?
The datasheet mentions that if a reverse current lasts longer than 5μs (typical), the chip will enter latched-off mode. What are the specific conditions for the chip to enter latched-off mode?