This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25170: Schematic review for LR2032 recharge circuit with MCU monitoring.

Part Number: BQ25170

Tool/software:

Hello I have designed the attached schematic using the BQ25170 for a battery charging circuit intended to be used with a LR2032 battery.

I would appreciate any feedback!

Features:
4.2V charge voltage

10mA charge current with RC filter on ISET

Charge enabled by MCU through TS pin

No temperature monitoring

STAT and PG pins monitored by MCU.

Battery voltage monitored by MCU.

N-channel FET used to enable battery monitoring to reduce current consumption.