Other Parts Discussed in Thread: TPS25751
Tool/software:
Hello,
I am designing a PCB that would require 5W per board, (5V with up to 1A of current). To power this board, I would like to use a USB C connector such that any off the shelf supply can be used. I would like to design these boards in such a way that they have two USB-C ports, where one acts as the source and the other can sink power to another board, such that multiple of these boards can be daisy chained together. Is this possible with the TPS65988 IC?
Thank you.
Sincerely, Jay