This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53513: Inquiry on TPS53513 EN-to-VOUT Startup Time Variation

Part Number: TPS53513


Tool/software:

Hi

I have been reviewing the TPS53513 datasheet and would like to clarify the EN-to-VOUT startup time.

According to Section 7.3.2 and Figure 33 (Power-up Sequence Waveforms),
When the EN pin voltage rises above the enable threshold voltage (typically 1.4 V), the controller enters its start up sequence.
The controller then uses the first 400 μs to calibrate the switching frequency setting resistance attached to the RF pin and stores the switching frequency code in internal registers.

However, during our testing, we observed that the total time from EN activation to VOUT output initiation consistently measures 1.129 ms,



・DATASHEET

Could you please confirm the following points?
・Is it acceptable that the total time from EN activation to the initiation of VOUT output is 1.129 ms?
・Is there a more detailed document on this, and is 400us the maximum value for the delay time?

Thanks and Best Regards

Chunli Liang