Part Number: BQ24133
Tool/software:
Hello, thank you as always for your help.
I have a question regarding charging behavior.
When I charged a 1,800mAh lithium-ion battery, the LED turned off properly upon full charge, as expected.
However, when I charge a 3,000mAh lithium-ion battery, it seems to reach almost full charge, but the charging current remains at around 600mA, and the LED turns off very briefly, then turns back on and stays on. This behavior repeats several times, and eventually, the LED enters a BLINK state.
Here, the fast charging current is 1.5A, and the TTC is HIGH.
I would appreciate your insight on this.
Thank you again for your continued support.





This photo shows the waveform of the SW pin during battery charging.