This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950 BKBAT worst case drain current spec.

Other Parts Discussed in Thread: TPS65950

Hello:

What is the worst case current drain specification for the TPS65950 BKBAT (M14 ball) input on hte TPS65950?

Thank you,

Frank

  • Hi Frank,

    This depends on your system. Ideally in backup the system would drain very minimal. In this mode only the 32K is active and the purpose is to maintain RTC. You can check the backup consumption, which i would guess you have already done (2.25uA + add minor margin). 

    You can use the above value for all calculations for your battery/super-cap/coin-cell.

    If the above does not help then please help understand your concern.