Tool/software:
Hello,
I am an FAE at a distributor of TI products, my customer has asked me about the LP3954.
The operating conditions and problem symptoms are as follows:
WLED1 and WLED5: Setting to 5mA
Assumes continuous operation for 3 hours per day for 20 days
When used for the above period in environments of 40°C and 60°C, the current value drops.
In short-term tests, the current value returns to normal when the ambient temperature reaches 25°C.
However, after 20 days of continuous operation, the current value remains low even when the ambient temperature reaches 25°C.
Is the current value still low because the IC is broken?
Or is it due to aging?
Please let me know your opinion.
Best regards,