Tool/software:
I'm trying to choose the capacitor that bypasses the Vcc pin of TPS61379.
I chose 220nF for the bootstrap capacitor. The application prose in the datasheet mentions that the capacitance of the Vcc capacitor needs to be at least 10x the capacitance of the bootstrap cap. In my case this would point toward the Vcc cap being 2.2uF.
I'm trying to determine whether I can make the Vcc cap a 0402 device. But it occurs to me that the voltage on the Vcc pin might be far higher than the input voltage for the IC. I believe that the boot strap cap pumps Vcc up above VIN, correct?
For a VIN roughly equal to the voltage on a fully charged lithium ion battery (~3.8V), what is the expected maximum voltage on Vcc? My output voltage is expected to be 5.2VDC.
Could I have chosen the boot strap cap to be 100nF instead of 220nF? This would make it easier to find a Vcc cap in a 0402 package.
Thanks from Indianapolis US.