This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24308: Fluctuation in BQ24308DSGR IC

Part Number: BQ24308


Tool/software:

Hi Ti,
   We are using the BQ24308DSGR IC. The issue is that when we connect the load, fluctuations occur. On the ILIM pin, we are using a 30.1 kΩ resistor, which limits the current to 1.5 A. We also tried using a 4.7 kΩ resistor to allow up to 2 A, but the fluctuations continue to occur. We would like to understand why this issue is happening.