This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3842: Questions about SMPS design

Part Number: UC3842
Other Parts Discussed in Thread: UCC28C56EVM-066, UCC28C56H

Tool/software:

Hi,

I’m working on designing an SMPS using the UC3842 IC.
My topology is a conventional flyback converter without any special techniques.

However, my input voltage range is from 200V to 1000V, and my output specification is 30W at 24V. My target efficiency is 90%.
I realize that the maximum input voltage is a bit high. I have looked for other controllers that can handle these requirements, but I haven’t found any, so I have to use this IC.

I would like to know if it’s possible to use this IC with my input specifications.
Additionally, I need over-voltage protection on the input and over-current protection on the output.

Could you please recommend how to implement these protection features?