This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5137F-Q1: Not starting up

Part Number: LM5137F-Q1
Other Parts Discussed in Thread: LM5137

Tool/software:

I am turning on the LM5137F-Q1 on a board of my own design for the first time and I am not seeing any output. The LM5137F-Q1 is configured for:

  • Single 12V output
  • 400Khz switching frequency
  • 14V UVLO turn-off
  • 16V UVLO turn-on
  • 4.6ms soft-start time
  • FPWM enabled
  • DRSS on
  • 27A Iocp (load is resistive heater, ~23.5A from both channels)

Can you please provide some guidance on what to look for to get the LM5137 up? I see the following:

  • VIN = 41.34V 
  • VDDA = 5V
  • VCC = 5V
  • EN1/2 = 2.48V
  • CNFG = 5V
  • PFM/SYNC = AGND
  • What other signals are important to know?

When the circuit is enabled, I see the output ramp to ~144mV then stop and try again.

 t