This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27427: QUESTION ABOUT BQ27427

Part Number: BQ27427
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

Hi team,

Here is FAE Chris, My customer Emdoor used BQ27427 in the AI ​​glasses project and encountered the following problems. Hope you can give some suggestions. 

Background: customer is using the Android platform, using a very similar CHEM-ID 3904, and has updated the QMax and Ra tables.

Questions:

1, When performing a discharge test at room temperature, it was found that the power suddenly jumped from 11% to 1%.

2, After restarting the machine, the displayed voltage value and the actual battery voltage are very different.

Best Regards

Chris