Part Number: TPS65130
Tool/software:
Hi Team,
I'm designing a DC/DC converter that uses 5V DC directly from the USB VBUS and is meant to output +/-15V.
The problem I'm having is that I have 0V at the output capactiors of the V_POS (+15V) and -5V at the V_NEG (-15V). Load-wise, I just have 350kohm load for the time being on each, which is nothing current-wise.
My schematic is as below:

My layout is as below:

I've also looked into other posts on this part number and I've also tried adding the 51kOhm resistor as suggested on TPS65130: Inverting converter is not regulating under load - Power management forum - Power management - TI E2E support forums and TPS65130: TPS65130 negative output issue - Power management forum - Power management - TI E2E support forums, however the result is still the same.
Some information on the components being used:
- Schottky diode: MBRM120LT1G
- PMOS: SI2323DS-T1-GE3
- L2/L3: NRS6028T4R7MMGK
Would it be possible to provide some guidance? Please let me know if any further information is required.
Thank you very much!