This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B4250-Q1: Output capacitor selection for TPS7B4250-Q1

Part Number: TPS7B4250-Q1


Tool/software:

Hello Expert, 

My customer is using TPS7B4250-Q1 and reviewing their external component with car oem.

She is using 2.2uF MLCC on the output of TPS7B4250-Q1. 

 

Datasheets specifies requirement of output capacitor as below. 

  1. VALUE : 1~50Uf
  2. ESR : 0.001 ~ 20 ohm

There're no comment about the frequency range of this ESR requires.

Could you please specify which frequency range the ESR should meet the requirement?

Thank you in advance.