This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40Z80 the program has flown

Part Number: BQ40Z80

Tool/software:

Dear

    Model: BQ40Z80. During mass production, 50% of the programs flew out. We confirmed with the customer that no locking action was taken because the production line needs to detect the board and the shipment status needs to be locked.

50% of the programs flew out and were reset. Half of them were normal, while the other half were not. The automatic welding of nickel plates is B+, B2, B4, B -, and then manually welding lines B1 and B3. Can you help confirm if there are any welding requirements