Tool/software:
Hi Team,
We are planning to develop a 48V to 5V(15A) ,7.5V(17A),12V(8.5A) and 24V(4A) converters (individual boards) using the LM5148 for a UAV application and i would like the schematic/pcb and the quickstart files to be reviewed before it goes into production. I can share the files on private chat/email for review.
I have a doubt on the quickstart for the 24V design i did, the external compensation calaculation gave me a 0pF suggestion for Cc2 cap. Is this ok? Because the PM calulcated is around 50.
Looking forward for a quick reply from your end.
Best Regards,
Noel Binny Abraham