Part Number: BQ27621-G1
Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Dear TI Support Team,
I am currently using the BQ27621-G1 fuel gauge IC in my product for a single-cell 18650 Li-ion battery (nominal 3.7V, full charge 4.2V). The ChemID is left at its default value 0x1202, which is recommended for the cell type I use.
However, I need to configure the gauge such that a battery voltage of 4.1V is interpreted as 100% State of Charge (SoC) instead of 4.2V. In my application, the charger terminates at 4.1V, so I want to define the SoC range as 0% at 2.8V and 100% at 4.1V.
I attempted to change the full charge recognition threshold using BQStudio, but even after the battery is fully charged to 4.1V and charging is terminated, the gauge only reports around 94–97% SoC, which is creating inconsistency in my system.
Could you please advise:
-
Is it possible to redefine the SoC mapping range, so that 4.1V is considered 100% SoC and 2.8V is 0%?
-
Can this be achieved through BQStudio or via I2C commands (if so, please share guidance or script format)?
-
Is ChemID 0x1202 still valid for this voltage range, or would a custom ChemID be required for accurate SoC estimation with a 4.1V charge ceiling?
Any direction you can provide for solving this behavior would be highly appreciated.
Best regards,
Tarek