Hi,
I'm woking on a DC Buck converter with UCC35702 pwm controlled by a DC level.
I made a simply test circuit to check the IC but actually i'm stuck about the pwm signal generation: I can't get the IC working propely.
The voltage settings seems to be under the behavior ratings (0,6V<VFF<3,2V; Vdd>UVLO start threshold), Vsclamp is set at 50% of Ct voltage ramp.
It starts the voltage ramp on the capacitor Ct, but nothing happens on the Output pin.
Cs of the SoftStart pin is always at 0.002V and it never charges on startup time.
For the test purpose Ilim and Count pin have been bypassed to gnd.
I can't figure out my fault.
Could you help me to get this circuit working?
Thanks a lot,
Raffaele