This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28050: design query

Part Number: UCC28050
Other Parts Discussed in Thread: PMP11155

Tool/software:

Hi 

Whether this UCC28050 part can be used for a single stage 105W flyback converter CV power supply for the below specification?

Input voltage: 90-264VAC

Output: 24V/4.2A

Efficiency: >90%

PF: >0.9

THD: <20%

Can you please confirm?

With regards

Rakesh.P