Part Number: BQ25176J
Other Parts Discussed in Thread: BQ25176, , BQ25170
Tool/software:
Hello,
I’m evaluating a battery with a thermistor connected to the BQ25176EVM board.
However, when the thermistor-equipped battery is connected, the PG LED begins blinking, and it appears that the constant current (38 µA) is no longer being supplied from the TS pin.
Upon inspecting the battery, I found that there seems to be a capacitor of approximately 0.1 µF connected in parallel with the thermistor.
Does the BQ25176 include any kind of timeout behavior where, if the TS pin voltage doesn’t settle within a specified range within a certain time, the current source is disabled?
If so, could you clarify what that timeout duration and the expected voltage threshold (perhaps V_TS_EN?) would be?
Any insights would be greatly appreciated.
Best regards,