This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR54410: Vin Voltage Rating

Part Number: LMR54410

Tool/software:

Hello, 

The Vin specification for the lmr54410 differs between the title in the datasheet and the description. Some times the maximal Voltage is stated 36V and sometimes 45V is stated. Which is correct?

Best Regards

Erik Wichmann

  • Hi Erik,

    It's ok to have transients above Recommended Operating conditions for a short period of time (few seconds), and it shouldn't affect long term operation. If you need a part that needs DC >36V for long periods of time, then I would recommend using a different part.

    Thanks,

    Andrew