Tool/software:
Hi team,
I just received a request form Elobau regarding this device.
This is not a concrete project but they are currently validating certain devices.
In this case They are aiming for the following setup:
__________________________________
I am currently evaluating the new TPS923650D2DRLR for a wide input voltage application.
Right now only early prototyping, so no numbers on yearly demand.
The input voltage might vary widely from 24 V to 48 V. The output voltage will be around 44 V, 0,5 A max.
Would this chip be a good fit?
Any suggestions for an inductor for this V_in range?
_________________________________
Can we recommend the right coil product for this?
Best regards,
Rosario