Tool/software:
I have some products that use the BQ24195. At the end of manufacturing assembly, the devices are commanded into shipping mode. At this point the power is disconnected from the VBUS pins while the battery stays connected and is at about 3.9 V. ON re-connection of 5 V to the VBUS pins, the PMIC will not power up.
The steps are:
- Product is powered from 5 V supply on VBUS and battery is connect at about 3.9 V. The PMIC is put into Shipping Mode. The product remians power until the 5 V supply is disconnected.
- In this unpowered state, REGN ~ 0 V (normal operation) and VBUS discharges to approx. 3 to 5 mV (proper conditions for the device to have powered down)
- The 5 V power supply is reconnected to the product and VBUS is measured to be approx. 5.05 V. The product does not power up and REGN remains at approx 0 V.
The only way to get the PMIC to power up again is to completely disconnect ALL power sources, including the battery, so that the PMIC returns to its factory settings (I am assuming that's what happens when the PMIC loses all power).
These products are using a lithium polymer battery that have a built-in temperature sensor, and the temperature sensor is connected to the TS pin of the PMIC. I'm looking through the BQ24195 datasheet to see if an out of range voltage at the TS pin prevents the PMIC from powering up again after shipping mode, but I haven't found those details yet. Can you tell me if an out of range TS voltage prevents the PMIC from powering up?
I read another similar post about a PMIC not exiting shipping mode but there was no resolution in that thread.
Can you suggest some reasons why the PMIC won't exit shipping mode?


This resulted in the error state;
This resulted in normal operation