Other Parts Discussed in Thread: TPD4S480, BQ25756, TPS26750
Tool/software:
Hi,
My customer is looking for an IC recommendation. Is there any IC that could combine USB 3.1 speed of 10Gbps and at the same time usb pd with extended power range (epr) up to 140W or 180W.
Or should we use two separate ICs one for power and one for data ?
They're interested in supporting 240W dual role and source for USB sticks
The power role should be sink 140W - 180W.
Appreciate the help on a recommendation, thank you!