Tool/software:
My design is using the TPS63900 along with some mosfets and resistors to change the current at which a supercapacitor charges. Below are current traces of switching between a 1mA limit and 2.5mA limit. The 2.5mA seems to consistently be about 3mA, but that is not the problem. On about 130 of 150 boards, the waveform looks like the first image. Nice and stable. However on about 20 of my boards, the waveform very consistently and repeatably looks like the 2nd picture. The average current is the same, but the waveform is very noisy. It is worth noting that the 1mA curve is very steady on all of the boards
I am hoping that someone can provide insight as to why this is happening and if this behavior is expected and/or if it will cause damage to the TPS63900.
Thank you