Tool/software:
LM5176's datasheet says that Vin's operating current is 2mA typ, 4mA max. (And based on the block diagram, I would think that whether it's Vin-only or Vin+Vbias, the total current into the chip would be nearly the same, right?)
Vin then feeds what looks to be a simple linear LDO regulator, which is VCC's 6.95-7.88V.
The datasheet also says VCC's current limit is 65mA.
If the linear regulator on Vin only takes in a max of 4mA, how is 65mA from VCC possible?
Or is the datasheet just saying that VCC has a built-in current-limiter, and it's set to 65mA?