Hi,
The load transient response is not like shown in the datasheet. I have checked it with the TPS780xxEVM-301 and on my board. When I am trying to pull 10mA I get a drop 215mV and not 100mV like shown in the TPS780xxEVM-301 datasheet. When I am trying to pull 100mA I get a drop 655mV. How can I get better performance? Is there somthing checked that I can use?
When checking the current consuption of the TPS780300250DRV with 0mA load current (open output) when I reach lower input voltages than 3000mV the input current rises to around 6uA. Is it a normal measurment?
Thanks.