Tool/software:
Hi everyone,
I'm currently working on a board that uses the TPS7A2533DRVR LDO, which should output a fixed 3.3V. However, I'm only getting 1.08V at the output.

To troubleshoot, I have desoldered the following components which were part of the feedback network:
-
R894
-
R1776
-
R1777
-
C2188
Since this is a fixed-output version, I understand that the feedback resistors are not required and FB pin should be connected internally.
Despite removing these components, the issue persists—I'm still measuring around 1.08V at the output.
I'm attaching the relevant portion of the schematic/layout here for review. Could anyone please help verify if the surrounding circuitry is correct and if there are any issues I might have missed?
clues : Input 5V and enable 5v is coming,
Any suggestions would be greatly appreciated!
Thanks,
Sai Kiran