Hi everyone,
I'm working on a 36V 15A Boost converter using the TI LM5122 controller and running into gate drive ringing (M3 & M4) and overlap issues under high load conditions, Causing Heat and Losses, Hoping someone here has seen this before and can offer insight.
Specs:
-
Controller: LM5122ZPWPT
-
VIN: 22–30V, 27V TYP
-
VOUT: 36V / 15A
-
MOSFETs: CSD18533KCS
-
Gate driver directly from LM5122 (no external drivers)
- Fsw : ~250KHz
- Webench Design: 5758.WBDesign59.pdf
Problem Summary:
At higher loads (10A+), I’m observing severe gate ringing, dead time overlap and heating of Mosfet, where both MOSFETs are briefly on — leading to MOSFET (M4) failure. This behavior isn't present at lighter loads. Attaching the Schematic
Original Sch :lm5122 Boost36V15A-1.rar
Modification done: Modifications lm5122 Boost36V15A-1.rar
What I've tried so far:
-
Removed MOSFET (M3) entirely and replaced with a fast Schottky diode (STPS30M60ST) — eliminated dead time issue and the failure of M4 but at a cost of power loss,
along with VDS Snubber (10R 470PF) Circuit for M4, still the gate ringing persists for M4
-
Added gate resistors (10Ω–60Ω range) — little to no improvement.
-
Tried gate diodes (to speed turn-on) — even more gate ringing
-
Observed that the Miller plateau dips significantly at higher loads, may be self-turn-on?
- Added Snubber (10R 470PF) for gate along with gate pull down resistor not much improvement.
Observations:
-
Strong oscillations during switching, especially on VGS.
-
Measured ~5–15 MHz ringing.
-
MOSFETs heat up quickly around 75degC at 10A for just a few minutes, Mosfets are mounted on a big heat sink box with air flow 27degC , the TAB is around 45degc
- The Power loss calculations say 40-50degC, agreed that bad rise and fall times are the issue, how to make it better?
Oscilloscope captures:
- The very beginning setup without any modifications: INITIAL VGS M4 1A.rar
- Dead Time : VGS of M3 and M4 : DEAD TIME.rar
- Current Stage : adding gate resistors, diode and snubber modifications, VGS of M4 at 1A and 10A load: VGS M4 1A.rarVGS M4 10A.rar
Questions:
-
Any proven techniques for damping gate ringing without slowing switching too much?
-
How to safely tune dead time in LM5122 to avoid cross-conduction?
-
Better snubbers values help across gate or drain-source?
-
Anyone used external gate drivers with LM5122 for stronger control?
- Better Gate resistor values? with proper calculations?
- Better Mosfets ? how about CSD19505KCS ?
Would appreciate schematics/layout feedback if someone has worked on high-current LM5122-based converters.
Also let me know if any other details required, I'm planning to make another layout.
Thanks in advance!
Arvind