This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: Thermistor connection shared between BQ27220 and BQ25170

Part Number: BQ27220
Other Parts Discussed in Thread: BQ25170,

Tool/software:

Hi

   I have used BQ27220 and BQ25170JDSGR for fuel guage and charger IC respectively in my system. I have connected BIN pin and TS pin of BQ27220 and BQ25170 IC respectively with thermistor (10K) to ground. Now the value 400mV in TS pin is not coming and charging gets intermittent (ON and OFF). Kindly suggest us for charging it properly. In one of our board it is working properly but in other boards it is not charging intermittently. In other boards after removing fuel gauge IC, charging is done properly,fyi

Thanks

R.Sivasuryan