This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: About parameter program

Part Number: BQ27220
Other Parts Discussed in Thread: GPCCEDV

Tool/software:

Dear Expert

Question 1: The OCV parameters in the OCV11.txt sent back by ti have a significant error compared to the actual values. Is there any way to optimize them.
Question 2: In the case where the gauge loses power and the FCC is lost every time, can we record the learned FCC in the MCU and write it back every time the power meter is powered on.

GPC CEDV tool, rev=61		
Configuration used in present fit		
ProcessingType=1		
NumCellSeries=1		
CellTermV=2700		
ChemType=1		
VoltageColumn=1		
CurrentColumn=2		
TemperatureColumn=3		
ElapsedTimeColumn=0		
FitMaxSOC%=12		
FitMinSOC%=6		
LearnSOC%=7		
		
CEDV parameters resulting from the fit. If EDVV bit is set to 1, EMF and EDVR0 have to be multiplied by the number of serial cells when written to data flash		
		
EMF	3402	
EDVC0	115	
EDVC1	0	
EDVR1	493	
EDVR0	2652	
EDVT0	3941	
EDVTC	11	
VOC75	3935	
VOC50	3808	
VOC25	3752	
		
		
Recommended SOC deviation tolerance at EDV2 point is  < 5% for low temperature and <3% for room and high temperature		
		
Deviations for this set of parameters are given below for each file		
		
file	SOC error, %	pass
roomtemp_lowrate.csv	-0.971464005905691	1
roomtemp_highrate.csv	-4.52499502979749	1
hightemp_lowrate.csv	-0.769013429803439	1
hightemp_highrate.csv	3.9296642349732	1
lowtemp_lowrate.csv	2.41399268216828	1
lowtemp_highrate.csv	-0.271039778343413	1
		
Deviations are within recomended range. CEDV parameters are suitable for programming the gauge		
		
SOC, %	OCV, mV
0	2703
10	3160
20	3260
30	3324
40	3379
50	3450
60	3543
70	3623
80	3707
90	3791
100	3864
C

And our electricity meter often loses power, so we can record the learned capacity in eerom by ourselves. Do you write it back when initializing the gauge during power on