Tool/software:
Hi,
The VU protection not work follow the below steps. UV protection is activated. (Settings / Protection / Enabled Protection A / Bit 2 Enable)
1.Power supply set 16 cells voltage to 2380mV.
2.Modify cell 2 voltage gain from 12122 to 11000, let read out voltage become 2143mV.
3.UV threshold is 44*50.6 = 2226.4mV
4.Min cell voltage is 2143mV which under threshold of UV but UV portection flag not acitve.
It seems that the condition for triggering UV is not based on the value read back.
What is the UV protection trigger conditions?
best regards,
Aska