Tool/software:
At room temperature, charging with 4.4V can correctly display 100%, but at 50℃ high temperature, charging with 4.2V can only reach 83%. This is because the battery cells can only be charged to 4.2V at high temperatures. May I ask if I also need to display 100% when charging at high temperatures? Is this achievable? The attachment contains the GG file and LOG data. Please help answer this. Thank you