Part Number: LM5180-Q1
Other Parts Discussed in Thread: LM5180
Tool/software:
I hope this message finds you well.
In my current design, I am using the LM5180 quasi-resonant flyback controller. The input voltage range is 30 V to 10 V, and I aim to generate two independent isolated 5 V outputs from this single converter. For this purpose, I have considered using the Würth Elektronik transformer with part number 750313974.
One of the outputs is expected to supply 400 mA, and the second output will supply approximately 100 mA. I would like to confirm whether this transformer is suitable for such a configuration and whether the output voltages can remain stable under these load conditions.
Additionally, I would appreciate your guidance on the following:
-
Are minimum loads required on the secondary outputs to maintain regulation?
-
Would you recommend an alternative transformer that may be better suited for this dual-output 5 V isolated design with the LM5180?
Thank you in advance for your support. I look forward to your insights