Tool/software:
Hi Folks,
We are having an issue with the BQ40Z80 which seems to perform unexpected resets every now and then. This happens while the battery is in discharge, usually at high amps but not always (20A/30A) communications stops with the BMS for 2 to 3 seconds before coming back.
When it comes back all values seems correct (voltage, current, ...) however the remaining capacity has jumped by 10 to 20% relative to its original value. I imagine that this is because on reset the chip performs a voltage reading to establish the current battery capacity, and since this is on a rather heavy load the voltage is not accurate.
How could we go around fixing this? Are there known issues or phenomenons that could explain those resets?
Just in case this can be useful: These battery are used in a redundant scheme (two batteries) connected through ideal diode circuits using the LTC4359. They drive a brushless motor that goes around 60A at max. The BQ40 is connected to an STM32 MCU for reading through the smbus.
Many thanks,