This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A94: Can the TPS7A94 be used as a variable voltage supply?

Part Number: TPS7A94


Tool/software:

I want to replace the LT3045 with the TPS7A94.  The LT3045 also uses a resistor between the SET pin and GND to set the VOUT.  A DAC output can also be connected to the LT3045 SET pin, so that DAC VOUT = LDO VOUT.  I need 0 - 3 V output and about 840 mA current.

Please tell me if I can connect a DAC output to the TPS7A94 NRSS input so that DAC VOUT = TPS7A94 VOUT.  Do you have an example circuit?  What should I be careful about?